Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The XBee3 Thing Plus is an ultra-capable and easy way for getting into wireless device development.
These paper-thin, adhesive EPCglobal Gen2 tags work with our RFID readers and can be stuck to practically anything.
RFM97CW Sub-GHz radio transceivers are ideal for long range wireless applications.
The Digi XBee® RR Pro Module is an embedded solution providing fast point-to-multipoint or peer-to-peer networking via an SM…
XBee RR 802.15.4 RF Modules are embedded solutions providing wireless end-point connectivity to devices.
The SparkFun Thing Plus - NINA-B306 offers a unique combination development platform in the Thing Plus form factor featuring …
These wireless receivers work with our 434MHz transmitters. They can easily fit into a breadboard and work well with microcon…
This is a similar XBee Pro module with a u.Fl connector. You also get a built in microcontroller so it can be programmed usin…
Commonly used to attach WiFi, Bluetooth, or nRFxxx based devices to a 2.4GHz antenna.
The Digi XBee® RR Pro Module is an embedded solution providing fast point-to-multipoint or peer-to-peer networking via an U.…
This is an XBee module with a U.FL connector. You also get a built in microcontroller so it can be programmed using MicroPyth…
The ESP32-C3 Mini Development Board is an entry-level development board based on ESP32-C3-MINI-1, a module named for its smal…
The SparkFun Notecarrier Cellular Function Board adds a cellular modem to the MicroMod ecosystem using the Notecard - NOTE-NB…
ESP32-C6 is Espressif’s first Wi-Fi 6 SoC integrating 2.4 GHz Wi-Fi 6, Bluetooth 5 (LE) and the 802.15.4 protocol.
SparkFun has teamed up with ARM and Dialog to provide you with this WiFi Shield based around the DA16200 module.
The Arduino Funnel I/O (Fio) is a board designed by Shigeru Kobayashi, based on the original design from [LilyPad](http://www…
PCB edge mount - SMA RF connector. Perfect for prototyping with the GPS and Cellular devices that require an antenna connecti…
Operating on the 2.4GHz or 5.8GHz band, it works great for WiFi, Bluetooth or ZigBee.
The SparkFun MicroMod DA16200 Function Board adds a fully integrated WiFi module to any MicroMod project.
The WiFi Shield gives your OpenMV Cam the ability to connect to the Internet wirelessly and is perfect for streaming video fr…
These wireless transmitters work with our 315MHz receivers. They can easily fit into a breadboard and work well with microcon…
Embark on a Journey of RFID Exploration with the SparkFun DataLogger IoT RFID Kit.
This is an XBee Pro module with an RP-SMA connector. You also get a built in microcontroller so it can be programmed using Mi…
The Edimax 2-in-1 Wi-Fi 4 & Bluetooth® 4.2 Adapter is a nano-sized USB Wi-Fi adapter that supports Wi-Fi up to 150Mbps.
These wireless receivers work with our 315MHz transmitters. They can easily fit into a breadboard and work well with microcon…
The ESP32-C6 has integrated 2.4 GHz Wi-Fi 6 (802.11ax) radio, and also supports the 802.11b/g/n standard for backward compati…
This is a simple breakout board for our RFID readers. The SparkFun RFID Reader Breakout converts the 2mm pins to bread board …
Raytac’s MDBT42T-AT is a BT 5.1 stack (Bluetooth® low energy or BLE) module designed based on Nordic nRF52805 SoC solution…
Jump-start your IoT development with the Omega2+ Starter Kit.
This is an adapter that converts an RP-SMA board to an SMA antenna. The adapter will connect to any of our 2.4GHz wireless bo…
The SparkFun AzureWave Thing Plus is a Feather form-factor development board equipped with the AW-CU488.
With Single-Board Computers (SBCs) on the rise, it is a good idea to have an easy way to interface with them. Operating on a …
WizFi360-EVB-Pico is based on Raspberry Pi RP2040 and adds WiFi connectivity using WizFi360.
If you need maximum distance for your LoRa project you need this incredibly durable, outdoor antenna with 5.8dBi gain.
The SparkFun MicroMod ESP32 Function Board adds additional wireless options to MicroMod Processor Boards that do not have tha…
The ESP32 WROOM MCU Module with PCB Antenna is a powerful, generic WiFi+BT+BLE MCU module that targets a wide variety of appl…
The SparkFun Wireless Motor Driver Shield is designed to make connecting motors, sensors and other components to your Arduino…
Designed for transmit and receive at 401MHz, this quarter-wave antenna is the perfect partner for our ARGOS ARTIC R2 satellit…
The Raspberry Pi Compute Module 4 represents a huge change for the Compute Module line. The biggest change being the move fro…
This is the Antenna Kit for the Raspberry Pi 4 Compute Module wireless variants.
WVR features 8GB of memory and an advanced Web GUI where users upload audio and manage configuration and firmware.
The RN-52 module from Roving Network is an audio module that provides a highly integrated solution for delivering high qualit…
The BGM220 Explorer Kit is an ultra-low cost, small form factor development and evaluation platform for the BGM220P Wireless …
The Particle Xenon is a low-cost mesh-enabled development kit.
It's best to think of the ESP32-S2 WROOM Module as the next step in the ESP32 WROOM module line.
The Raspberry Pi Compute Module 3+ contains the guts of a Raspberry Pi 3 Model B+ with 8GB of eMMC Flash memory.
The ESP32-WROOM-DA module achieves high-quality, wireless connectivity across large areas, using two complementary PCB antenn…