Deck out your Sphero RVR robot with a Raspberry Pi Zero W, remote pan-tilt camera, and some Qwiic components!
Two GPS boards utilizing the NEO-M9N module are now available, along with the new Cthulhu Shield
A new Qwiic Pi SHIM is here, as well as a new version of our classic LED Starter Kit and a 976x592 CMOS Camera!
The High Precision Temperature Sensor is now in full production! We also have a new machine imaging camera designed specifically for the SparkFun Edge Dev Board!
Let's take a quick look at the current offerings of the popular LIDAR-Lite from Garmin!
I'm using six of the same sensor in my fiber optic suit, with only four hardware configurable addresses. I need to take advantage of my ESP32 to create multiple I2C buses.
When it comes to proximity and distance sensing, LiDAR has a lot to offer. With Garmin's LiDAR-Lite v4, there are some new features and advances you're definitely going to want to see.
Many of us at SparkFun consume coffee for breakfast, maybe lunch or dinner, but for some go-getters it's all three. Join me as I dig into the habits and trends of our breakroom coffee setup.
The new A111 Pulsed Radar Breakout is looking good in red! We also have a new kit that makes it easy to get started with micro:bit!
What do you do after the SparkFun Inventor's Kit? The world of electronics using Arduino is vast – here are a few tutorials to help take your projects to the next level!
A new biometric Qwiic sensor is here! We also have a new electric screwdriver and a USB Power Meter.
The trail-ready lightning detector has been out in the wild getting some good use. As summer nears its end, it is a great time to take the project back to the drawing board and figure out what should be upgraded, what should be added and what can be removed – just in time for some fall outdoor adventures!
After a short time in retirement, the SparkX A111 Breakout Board is coming back to life as part of the Get Sparked program!
New versions of the Teensy Audio Adaptor and the EasyVR 3 Shield are here, along with a new HC-SR04 Distance Sensor and a SparkFun-made 16GB NOOBS Card.
We've revised our AS3935 Lightning Detector, and we have a new Level Translator Breakout!
A Qwiic-enabled Ambient Light Sensor is here, along with an updated LilyPad LED board!
We recognize the pun and will not apologize. A new 9DoF IMU is here, along with a capacitive fingerprint scanner and a few other new products!
Congratulations, this history is motivational, Best regards from Queretaro Mex.