Unleash the power of WIRELESS electromyography and, almost paradoxically, we also have new flexible USB cables, extenders, and XRP connectors!
Our new Ultrasonic Distance Sensor brings a new ranging sensor option to the Qwiic Ecosystem. We also have two new Espressif networking boards!
The new SparkFun Optical Tracking Odometry Sensor is here with a slew of other new products, including two from our friends at FGSensors.
The new SparkFun M7E Hecto Simultaneous RFID Reader is here along with some new project mats from iFixit!
It's an assortment of new products from some of our favorite friends in the industry!
The brand new MyoWare 2.0 Wireless Shield is now available! With it we also have a new programmer board for your ESP32 WROOM Modules.
The Digi XBee Sensor Lab demo gets beyond the basics and showcases eight use cases, including connected agriculture, access control, and asset tracking, leveraging Qwiic sensors and Digi Remote Manager.
SparkFun's newest Thing+ board is here, equipped with the powerhouse ESP32-C6 module and it's accompanied by the new MOSFET Power Switch and Buck Regulator! That's not all, though, because all XRP Kits parts are now available individually!
Our newest RTK surveyor is here and it utilizes the mosaic-X5 from Septentrio! Be sure to also check out our new ISP Pogo Adapter and Qwiic 24 Bit ADC.
The BlueSMiRF v2 is now available with or without headers attached, along with a new Soldering Kit featuring the PINECIL soldering iron.
The newest Digi XBee® modules are now available at SparkFun Electronics, and we have new boards to support them!
The SparkFun LTE Stick, which utilizes the LARA-R6 from u-blox, is now available to transmit voice AND data over cellular IoT in North America.
The ESP32 Qwiic Pro Mini and AS7331 Sensors are here along with a new GPS Dead Reckoning Kit and a handful of other new products from our partners.
Silicon Labs created some amazing project examples, using the SparkFun Thing Plus Matter board, that you can follow once you've got yours up and running. Including gesture recognition and image classification using TensorFlow Lite, counting people in a room, creating an RFID door lock system, and connecting the SparkFun Thing Plus MGM240P to an Android device, these examples are sure to inspire you!
We've assembled this annotated resource list to better understand Matter and Thread - what it is, why it matters, and use cases.
The Qwiic Dynamic NFC/RFID Tag graduates to reds and the AWS IoT ExpressLink SARA-R5 Starter Kit gets a new version.
Congratulations, this history is motivational, Best regards from Queretaro Mex.