Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
Are you a Java developer looking to add advanced hardware I/O capabilities to your Android or PC application? Well then the I…
This is the same product as the [ProtoShield Kit](https://www.sparkfun.com/commerce/product_info.php?products_id=7914). The d…
What can you do with the Raspberry Pi, the inexpensive credit card-sized computer? All sorts of things! If you're learning ho…
**Replacement:**[LCD-11315](https://www.sparkfun.com/products/11315). 4D Systems has released a new revision of this product!…
These 1.375" long stainless steel D-Shafts have a diameter of 1/4". The flat edge that runs the length of the shaft makes it …
This is a 1kg (2.2lb) reel of 3mm blue PLA plastic filament for 3D printing. PLA is a great general purpose filament with gre…
It's that time of year when we sell off our production scrap. These board do not work, but they make for great practice, and …
This is a very simple RJ45 PoEthernet MagJack connector that can help connect you to the Internet with the ability to provide…
**Replacement:** None. We are no longer carrying this t-shirt in our catalog. This page is for reference only. More swag? Wh…
**Replacement:** None. We are no longer carrying this adapter in our catalog. This page is for reference only. This is an ad…
This is a monolithic SMD 2.4GHz antenna. Works well for any 2.4GHz application, including WLAN, Home RF, and with Bluetooth®…
ADC 9 Click is 8th channel analog to digital converter expansion board.
If you already have or are looking to own some Circuit Stickers from Chibitronics you may be looking to add a few effects to …
**Replacement:**[DEV-11021](http://www.sparkfun.com/products/11021). The Arduino Uno has a new R3 version. It breaks out a fe…
The NCP303 is an ultra−low current voltage detector that contains a programmable time delay generator. These devices are sp…
Why not prototype in 3D? The SparkFun square-shape perf board is a roughly 2cm on a side with 0.1" spaced holes. Use it to cr…
The Digital Sandbox (DS) is a learning platform that engages both the software and hardware worlds. It’s powered by a micro…
The Distance Cubelet detects how far it is from an object. It uses infrared light and is accurate between 10 and 80 cm. The s…
Charger 13 Click is a single lithium-ion (Li+) cell battery charger.
**Replacement: **[COM-09636](http://www.sparkfun.com/products/9636)**.** We are discontinuing this line of Luxeon LEDs. We wi…
**Replacement:**[WRL-10535](http://www.sparkfun.com/products/10535). We are now carrying the same transmitter from a differen…
**Replacement:**[PRT-09682](http://www.sparkfun.com/commerce/product_info.php?products_id=9682). This has been replaced with …
In physical computing it's sometimes nice to know how physically close you are to an object. In other words, you may need to …
This is a pack of 2 wheels, specifically designed to mate with the RFL motors. Comes as a pack of 2.
The Brightness Cubelet has an analog photocell that responds to varying light conditions and detects the amount of light hitt…
nGen is a co-polyester Filament that is optimized for 3D printers and perfect for both prototyping and production. With high …
**Replacement:**[DEV-10174](http://www.sparkfun.com/products/10174). This kit now includes the Arduino Uno. This page is for …
If you need some juice, this 6Ahr triple pack is for you. These are very slim, extremely light weight batteries based on the …
There is really nothing like a well-designed project enclosure. Really, a clean enclosure can add a lot to a project. This cl…
Surface mount vertical 5-pin 1.0mm pitch connector for connecting to the EM-408 interface cable.
**Description**: This is the SMD connector for the PSP touch screen. 4-pin right angle good, friction fit connector with 1 mm…
The LilyPad XBee is a breakout board for the popular XBee modules that can be sewn into your e-textile projects to provide th…
This new version breaks out the PI09, FORCE WAKE, and the hardware reset lines. It also has a different crystal and uses the …
The Intel® Galileo Gen 2 board is based on the Intel® Quark SoC X1000, a 32-bit Intel Pentium®-class system on a chip (SoC…
**Replacement:**[DEV-11055](http://www.sparkfun.com/products/11055). We've run out of the V2s, but you can still get the late…
**Replacement:** None. We are no longer carrying this product in our catalog. This page is for reference only. This is the i…
Is there anything an Arduino can't do? Well, for one, most of them can't be powered directly from a 3.7V LiPo battery; much l…
If you want to get some sound out of your project but have a tight space budget, this is a good way to do it. This 0.25W, 8Oh…
**Replacement:** None. It's time for this product to step aside and make room in the catalog for even more cool stuff. This p…
The MaKey MaKey is really cool, but wouldn't it be cooler if it wasn't tethered to your computer? There's only one way to fin…
EL wire, or electroluminescent wire, is a flexible wire coated in phosphor. Apply the appropriate voltage and it lights up! E…
This is a very useful panel-mount locking button/switch. Press it once for 'on', once again for 'off'. It is a SPST N.O. with…
The SparkFun JPEG Trigger interfaces with the [LinkSprite JPEG Color Camera](http://www.sparkfun.com/products/10061) to simpl…
**Replacement:** None. There is no drop-in replacement for this part, but have a look at our cellular category for other modu…
The Knob Cubelet has a potentiometer embedded in one of its faces. It outputs a 0 when turned fully counterclockwise, and a 1…