Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
Ready to add audio to your next project? This small breakout board couples a small electret microphone with a 100x opamp to a…
**Replacement:** None. We have retired this product. This page is for reference only. This new version fixes the pinout for …
This is the Parallel Gripper Kit A, a simple and durable robotics kit that is great for "getting a grip" on pretty much any r…
EL wire, or electroluminescent wire, is a flexible wire coated in phosphor. Apply the appropriate voltage and it lights up! E…
**Replacement:** None. As we transition our stock of irons from Aoyue to Hakko, we'll be retiring the Aoyue compatible tips. …
The XS1 family of devices features a multi-threaded processor architecture constructed from XCore processors connected by com…
The GN3S Sampler v3 is a very interesting high-end research device. Co-developed by the [GNSS Lab](http://ccar.colorado.edu/g…
**Replacement:** None. We do not have a direct replacement for this part. This page is for reference only. This faceplate is…
The Inverse Cubelet calculates a value that is the opposite of the values it receives. Specifically, the Inverse Cubelet will…
The Blocker Cubelet is a basic building block that "blocks" data from its neighbors. It still passes power, but effectively s…
Fingerprint scanners are awesome. Why use a key when you have one right at the tip of your finger? Unfortunately, they're usu…
Need to autonomously monitor for that specific color value? Want to hone in on that magenta ball? Or follow that aquamarine l…
This is a breakout board for the ISD1932, a multiple-message record/playback device. This single chip can record up to 64 sec…
**Replacement:**[DEV-10908](http://www.sparkfun.com/products/10908). The new version of this board got some minor hardware ch…
The Distance Cubelet detects how far it is from an object. It uses infrared light and is accurate between 10 and 80 cm. The s…
EL Inverters, if you are wanting to do _anything_ with EL lighting you need one, period. This 3V EL Inverter is a special typ…
**Replacement:**[SEN-10742](http://www.sparkfun.com/products/10742). The new version has a more robust tube power switch and …
The Knob Cubelet has a potentiometer embedded in one of its faces. It outputs a 0 when turned fully counterclockwise, and a 1…
**Replacement:** None. We are no longer making this board but check out the rest of our Arduino-compatible [development tools…
Our friends over at Adafruit have made this nifty, little breakout using one of SHARP's silver monochrome memory displays. Th…
**Replacement:** None. We are no longer carrying this product, but check out the rest of our [e-textiles section](https://www…
We can't tell what [metallic salmon](http://en.wikipedia.org/wiki/Color) looks like, but this very small sensor can! The ADJD…
**Replacement:** None. We are no longer carrying this evaluation board in our catalog. This page is for reference only. The …
These aluminum beams are great for making unique links and connections in your [Actobotics](https://www.sparkfun.com/pages/Ac…
These blue “skate” wheels have an outer diameter of 2.975”, an inner diameter of 0.87”, and a width of 0.94”. When …
Do you need "Mega" power in a "Mini" package? We can do that! We're continuing our Pro series of Arduino-compatible microcont…
Need a smaller way to add some 'twinkle' to your LilyPad project? Then you need some LilyPad Micros! A LilyPad Micro is like …
These blue precision disk wheels have an outer diameter of 4”, a width of 0.23”, and utilize the 0.77” hub pattern. The…
These hub mounts mate directly to [Actobotics](https://www.sparkfun.com/pages/Actobotics) channels in multiple positions and …
These smooth (round) belts have a Durometer hardness of A70 and can withstand temperatures from -35 to 250 degrees F. Their e…
Who doesn't love the soft glow of electroluminescence? This EL panel is a flexible plastic sheet which contains a phosphor la…
These LED string lights are a great way to add light to any project with little to no soldering required. The insulated strin…
**Replacement:**[RTL-11082](https://www.sparkfun.com/products/11082). This board has been replaced with our Si4703 Evaluation…
**Replacement:**[COM-09603](http://www.sparkfun.com/products/9603). Although there is not a drop-in replacement, the BMP085 i…
These non-flanged "608" sized ball bearings fit nicely into a 22mm diameter hole and has a 8mm bore. This makes it perfect fo…
Two pin, compact surface mount connector. We really like the solid locking feeling and high current rating on these small con…
The BD10KA5W is a low-saturation regulator with an output voltage precision of ±1%. It also has built-in overcurrent protect…
These white precision disk wheels have an outer diameter of 2”, a width of 0.23”, and utilize the 0.77” hub pattern. Th…
It's your basic green action button! This is a very useful, small, panel-mount momentary switch. It is a SPST N.O. with the t…
This is a simple to use light sensor that outputs an analog value from 0 to 5V. With exposure to daylight, this sensor will o…
This is a 1kg (2.2lb) reel of 3mm red PLA plastic filament for 3D printing. PLA is a great general purpose filament with grea…
Six pin JST connector with white, 5 inch wire outs. Connector is 2mm, NOT Standard 0.1" spacing.