Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
The SparkFun Photon Wearable Shield makes it easy to add the WiFi enabled Photon to any wearables project. Each pin on the Ph…
Secure 4 Click includes the ATECC608A, a secure CryptoAuthentication™ device from Microchip.
The tools provide users the ability to apply the right amount of leverage and torque in order to get the right bend.
The SparkFun BlackBerry Trackballer Breakout gives you easy access to a trackball which measures up, down, left, and right mo…
This pamphlet is a sales sheet for retailers to use for their retail displays. Have them for customers as informational take-…
**Replacement: **None. There is no direct replacement for this product. This page is for reference only. Check the customer …
**Replacement:** None. We are no longer carrying this mug in our catalog. This page is for reference only. Coffee and beer s…
Environment 2 Click is a compact add-on board containing best-in-class SHT humidity and SGP air-quality sensing solutions fro…
**Replacement:** None. We have retired this product and carry no direct replacement. The Beagleboard xM, however, has many of…
LED Driver 4 Click is a form of a high-efficiency boost converter that is ideally suited for driving an array of white LEDs.
Main component on 6DOF IMU 11 click is the KMX63 from Kionix (ROHM company), a tri-axis accelerometer, tri-axis magnetometer,…
This is the Multi-Chassis Tank Kit, an easy to assemble and use robot chassis platform. The Multi-Chassis kit provides you wi…
MIKROE Proximity 12 Click is a compact add-on board that contains a high-performance light and proximity sensing solution.
TFmini Click is an adapter Click board™ used to interface a compatible ToF (Time of Flight) LiDAR sensor with the host MCU.
Brushless 8 Click is a compact add-on board suitable for controlling BLDC motors with any MCU.
BLE TX Click is a compact add-on board that contains a low-energy Bluetooth transmitter.
DC MOTOR 2 Click carries the TB6593FNG driver IC for direct current motors, from Toshiba.
MIKROE H-Bridge 8 Click is a compact add-on board that contains H-bridge current regulator.
PHT Click is a compact add-on board that contains a PHT combo sensor.
The main component of the Boost-INV Click is the LT3582, programmable boost and inverting DC/DC converter with OTP memory, fr…
Audio Xover Click is an analog active crossover solution for two-way loudspeakers.
These GoPro camera mounts provide you with a simple and lightweight way to attach your Hero 3 to your [Actobotics](https://ww…
The Kinoma Create V2 is the JavaScript-powered construction kit perfect for prototyping smart consumer electronics and Intern…
This Neon Flex Rope is a ~6.5ft (2m) long, non-addressable LED strip simulates the neon effects that you see in store fronts …
Hall Current 13 Click is a compact add-on board that provides economical and precise AC or DC current sensing solutions.
Who wants pi? The Raspberry Pi has made quite a splash since it was first announced. The credit-card sized computer is capabl…
This heavy-duty, 3-pole, double throw toggle switch is rated for up to 15 Amps of current. It can be panel mounted with a 7/1…
The Nordic Thingy:91 is an easy-to-use battery-operated prototyping platform for cellular IoT using LTE-M, NB-IoT and GPS. It…
Everything you need to build a robot.
Smart Sens 2 Click is a all-in-one self-learning AI smart sensor solution that contains multiple sensors.
Capturing high-definition video is a challenge for any project, but a great way to see where you're project has been, especia…
If you're looking to play with PICAXE microcontrollers on a computer with only USB, look no further! The PICAXE USB programmi…
HAPTIC 2 Click is a compact add-on board that contains a linear vibration driver.
**Replacement: **None. There is no direct replacement for this item, it has been discontinued. This page is for reference onl…
This is the littleBits Space Kit, a unique electronics kit for beginners and experts alike that contains everything you need …
Tynker and BBC Learning take coding to the next level with a programmable HiFive mini-computer and guided lessons covering Bl…
MIKROE Altitude 6 Click is a compact add-on board that allows height measurement of an object or point related to sea level o…
Spectrometer 2 Click is a compact add-on board that collects light waves.
A really cool rechargeable Lithium Ion coin cell battery. The battery is rated for 3.6V @ 110mAh - a great way to run a small…
**Replacement:**[GPS-10922](https://www.sparkfun.com/products/10922). The Copernicus GPS module is EOL and has been replaced …
The Boost 6 Click is a Click board™ which features the TPS55332-Q1, a monolithic high-voltage switching regulator with inte…
These un-threaded aluminum clamping hubs are perfect for standard applications that need shafting or tubing 1" in diameter se…
If you've never soldered before, this is the class for you! We've been teaching soldering a lot over the past few years - now…
Hall Current 7 Click is a compact add-on board that provides economical and precise solutions for AC or DC current sensing.
This is the same product as the [Mr. Roboto Kit](https://www.sparkfun.com/products/11257). The difference is this version com…
These continuous rotation 2:1 gear ratio channel gearbox kits incorporate threaded side mounts to easily attach a standard si…
**Replacement:** None. Although we don't have a direct replacement for this board, we have many IMUs in the [IMU category](ht…
**Replacement:** None. This product was retired because of supplier discontinuation. There is not a direct recommended replac…