Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
**Replacement:** None. There is no direct replacement for this board. This page is for reference only. Custom header board f…
This handy little IC will correctly and safely charge our Lithium Polymer batteries with power from a USB port or from a DC w…
**Replacement:** None. Due to poor sales, we have decided to remove this item from our catalog. This page is for reference on…
This is a crimp pin for the ZH-6 JST [connector](http://www.sparkfun.com/commerce/product_info.php?products_id=9690), which c…
**Replacement:** None. Unfortunately the supplier for these helical GPS Receiver is no longer in business so we can no longer…
**Replacement:** None. Unfortunately we no longer stock the Open Heart Kit. This page is for reference only. The Open heart …
Pianos are heavy and can take about a year to make. What if you could have one that weighed only a few grams and took a very …
The Magician Chassis is our latest robot platform from Dagu. It features two gearmotors with 65mm wheels and a rear caster. T…
Want to control a standard wall outlet device with your micro controller, but don't want to mess with the high voltage wiring…
Knobs are a great way to finish off your project and make it easier to adjust the level of your death ray. This knob mates to…
**Replacement:** None. We have unfortunately retired this product but you can always read about [how we built it](https://www…
**Replacement:** None. We no longer carry this poster in our catalog. This page is for reference only. This is the official …
**Replacement: **None. We are not currently selling the manual separately. But you can download and print it yourself. Check …
The Digital Sandbox Lab Pack includes 10 complete Sandbox kits and 10 add-on packs. The kit has everything you need including…
This is our version of the [OpenServo](http://www.openservo.com) open-source servo controller board. It's meant to replace th…
No mad scientist is complete without a quality lab coat! Make sure you're working in style next time you're in the lab tinker…
This was a great board but we made it better! Checkout the new version, [BlackBoard C](https://www.sparkfun.com/products/1509…
The RN-52 Bluetooth from Roving Networks is an audio module that makes it simple for you to create a hands free audio system …
**Replacement:**[WRL-10421](http://www.sparkfun.com/products/10421). This new version is a Series 2 which uses a much newer f…
**Replacement:**[SEN-11282](https://www.sparkfun.com/products/11282). We've made some minor hardware changes including the ad…
EL wire, or electroluminescent wire, is a flexible wire coated in phosphor. Apply the appropriate voltage and it lights up! I…
This is the LilyPad USB Plus, a sewable electronics microcontroller board controlled by an ATmega32U4 with the Arduino bootlo…
The Bluetooth Mate 4.0 is the next evolution in our line of serial Bluetooth modules. This board is equipped with an HM-13 mo…
Accel 10 Click features an ultra-low power triaxial "femto" accelerometer sensor with embedded intelligence, labeled as the L…
The PCM1803A is a high-performance, low-cost, 24-bit stereo analog-to-digital converter that can sample as high as 96k. The P…
**Replacement:** None. We are no longer able to get these. This page is for reference only. Hobbykings T6A 2.4GHz system is …
This is a USB 2.0 type A to Mini-B 5-pin cable, the most common mini-B connector that usually comes with USB Hubs, Cameras, M…
_There Are No Electrons: Electronics for Earthlings_ is an astounding book that provides the clearest and most entertaining i…
We all know that you can never get too many LEDs. Don't worry, we've got you covered. This is a mixed pack of 26 LEDs all con…
**Replacement:** None. We're not carrying this part anymore, but check out the rest of our [accelerometer ](https://www.spark…
**Replacement: **[DEV-09873](http://www.sparkfun.com/products/9873). We're fresh out of the 'old-school' version but you can …
**Replacement:**[BOB-10496](http://www.sparkfun.com/products/10496). This board had errors with the pinout of the connector. …
Have you ever needed a cheap way to activate something from across the room? Infrared remotes are still the cheapest way to w…
**Replacement:**[KIT-10547](http://www.sparkfun.com/products/10547). The new version of this kit is easier than ever for the …
This is a breakout board for the 100-pin TQFP package of Atmel's ATxmega128A1. The ATxmega128A1 is a low power, high performa…
**Description**: The LS20031 GPS receiver is a complete 10Hz GPS smart antenna receiver, that includes an embedded antenna an…
The TB6612FNG Motor Driver can control up to two DC motors at a constant current of 1.2A (3.2A peak). Two input signals (IN1 …
These 12" long stainless steel shafts have a diameter of 1/8". These shafts are solid, which makes them an ideal choice for a…
This is the retail version of our FTDI Basic 3.3v. This is the same as our regular FTDI Basic, but in retail packaging. T…
This is a simple three wire cable. Great for jumping from board to board or just about anything else. There is a 3-pin Molex …
These 6" long aluminum tubes have an outer diameter of 5/8", an inner diameter of 0.569", and a wall thickness of 0.028". Whe…
This is the same product as the [HMC5883L Breakout Board](http://www.sparkfun.com/products/10530). The difference is this ver…
Metal long standoffs: 1" long x 1/4" OD. Used to get your proto board up off the table. #4-40 thread. Fits most development b…
This is a breakout board for Freescale's MMA7361L three-axis analog MEMS accelerometer. The sensor requires a very low amount…
This is a blank faceplate for the Chameleon 1 enclosure system for development boards Having blanks lets you drill or nip w…
This is a breakout board for the DS1077 is a dual-output, programmable, oscillator. Contains a filter capacitor and all 8 pin…
**Replacement:**[BOB-10653](http://www.sparkfun.com/products/10653). We've added an on-board microphone and output speaker ja…
**Replacement:** None. We do not have a direct replacement for this tip. This page is for reference only. Shiny new tips for…