Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
POT 3 Click is a Click board™ with the accurate selectable reference voltage output.
**Replacement:** None. We do not have a direct replacement for this product. This page is for reference only. Schemer is a t…
This is a basic 16 button keypad that has been designed for easy user input and functionality.
**Replacement:** None. There is no direct replacement for this board. This page is for reference only. This is a breakout bo…
**Replacement:** None. We're not selling these battery holders anymore. This page is for reference only. The watertight batt…
These crimping pliers allow you to easily make your own wiring harnesses using crimp pins and cable housings. These are not a…
Meet Mr. Roboto! He's an Arduino-compatible development board designed to be used as a teaching tool for Arduino programming.…
We've all seen toys and things that change color when you run them under warm water or heat them up in the sun. Some of us we…
The SparkFun Inventor's Kit for the Genuino 101® board is a great way to get started with programming and hardware interacti…
Conductive thread is a creative way to connect various electronics onto clothing. This thread can carry current for power and…
**Replacement:**[KIT-11227](https://www.sparkfun.com/products/11227). We've overhauled the SIK Manual with new graphics, revi…
**Replacement:**[DEV-11226](https://www.sparkfun.com/products/11226). This kit now includes the Arduino Uno R3. This page is …
This is the retail version of our popular ClockIt soldering kit. This is a great kit to learn the basics of soldering. ClockI…
The PodSocket v1.0 pulls all 30 pins from the female dock connector and makes it easy to attach wires. This includes the PodS…
MIKROE CapSense Click add-on board features a capacitive sensing module CY8C201A0.
**Replacement: **None. We are no longer carrying this OLED module. This page is for reference only. If you need a small simp…
Here is a breakout board for the LS20126 GPS receiver. The board allows you to access all the pins on the GPS module through …
**Replacement:** None. Maker Faire is over, we don't have any more tickets. And even if we did have tickets, there's no show …
**Replacement:** None. We are no longer carrying this LCD module. This page is for reference only. E-paper displays are rad.…
This is the 26-pin SMD connector that mates with our e-paper character displays. **Note:** The tab on this connector may be …
Here is a three pin horizontal 1.0mm pitch connector. It is useful if you need something very tiny as a connection. These are…
Got an idea for a prototype but not sure exactly how to make it happen? SparkFun Electronics is offering five days of prototy…
The RFM22B is a low-cost ISM FSK transceiver module which offers communication at 433MHz ISM and adjustable output power of u…
The EasyUSB gives your microcontroller access to 2MB that can be seen as a mass storage device in most operating systems. Now…
This is a glass ferrule type fuse. It fits great with our 5mm fuse clips. The fuse is rated for 250VAC, up to 200mA. Fuses ar…
**Replacement:** None at this time. We are no longer carrying the Seeeduino FILM in our catalog. This page is for reference o…
This is a simple 8" long 2.5mm audio cable. It is terminated with a 2.5mm audio plug on one side and unterminated with bare w…
These alligator clips are useful for smaller wires that you don't want to deform. The clip has smooth flat metal blades that …
The same vibration you get when you receive a text message or phone call can be brought to your project using the Zio Haptic …
The Intel® Edison is an ultra small computing platform that will change the way you look at embedded electronics. Each Ediso…
We don't want to hype this solder TOO much, but this could possibly be the best solder in the world. There, we've said it. Th…
The new version of the Ardubot PCB breaks out all the Arduino pins to a separate row of headers. It also includes spaces for …
We're clearing out this black SparkX version so get the deal while you can. This version is identical to the red version (wit…
**Replacement:**[DEV-11608](https://www.sparkfun.com/products/11608). The Netduino Plus 2 is here! This page is for reference…
Do you dream of basking in the glow of 8-Bit VGA? Dream no longer, my friend. The Papilio VGA Wing has all of the hardware yo…
**Replacement:** None. We are reordering these without the wall wart. We will not be getting any more of these. This page is …
Here is a four pin horizontal 1.0mm pitch connector. It is useful if you need something very tiny as a connection. These are …
The HiFive1 is a low-cost, Arduino-compatible dev board featuring the Freedom E310 making it the best way to start prototypin…
The GP-635T is a slim GPS receiver with -161dBm tracking sensitivity and only 27 second cold start time. The slim design make…
EL wire, or electroluminescent wire, is a flexible wire coated in phosphor. Apply the appropriate voltage and it lights up! I…
Here is a five pin horizontal 1.0mm pitch connector. It is useful if you need something very tiny as a connection. These are …
This simple Transistor Array pack contains three SMD ULN2803 ICs from Texas Instruments. Each of these tiny ICs consists of e…
**Replacement:** None. We do not have a replacement for this part. This page is for reference only. Here is a simple fiber o…
**Replacement: **[TOL-11456](https://www.sparkfun.com/products/11456). We've found a supplier for a higher quality USB wall c…
**Replacement: **None. We are no longer stocking this shield. This page is for reference only. The Video Game Shield is an A…
The Spectacle Director Board controls all the actions in a Spectacle project. Though the Director Board doesn't do too much o…
**Replacement:**[TOL-10243](http://www.sparkfun.com/products/10243). We know you can't get enough of the special blend, but w…