Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
**Replacement: **None. We are no longer carrying this item, but have a look at the rest of our [development tools](http://www…
**Replacement:** None. There is no direct replacement for this item. This page is for reference only. This is a great lookin…
These shaft-mountable aluminum timing pulleys use XL timing belts and attach to a 6mm output shaft with a set screw. They hav…
Have a project that needs some good power? Do you like free power provided by our friend, Mr. Sun? Check out this high qualit…
This is a Ding and Dent version of our Raspberry Pi B Block for the Intel® Edison. This block has headers pre-soldered on, w…
This is a strip of 10 pieces of the black SMD Qwiic connector. This connector is used on all our Qwiic based boards. Use it t…
**Replacement:** None. We are no longer carrying this retail Digital FM Radio Receiver in our catalog. We are still carrying …
Arduino is the open-source electronics prototyping platform that’s taken the design and hobbyist world by storm. This thoro…
**Replacement:** None. We are no longer stocking these programmers. This page is for reference only. The PIC-PG3B is a power…
This is the PIC16F877A SMD IC Flash Microcontroller. This little chip was once used in our old Wall Clock Controller and whil…
The Eagle Schematics and PCB Layout course is the second course in the new SparkFun class series. In this hands-on class we w…
The Shapeoko 4 XL is a 3-axis CNC Machine kit that allows you to create your 2D and 3D designs out of non-ferrous metals, har…
Replacement: WRL-12581. The firmware on all our Roving Networks products has been updated from version 4.77 to the 6.15 versi…
The GP-2106 is a really tiny GPS module. It's so small, in fact, that it's almost too small to use. Not only that, but the 1.…
These standard gearmotors are incredibly tough and feature full metal gears to help you drive wheels, gears, or almost anythi…
This is a very small, extremely light weight battery based on the new Polymer Lithium Ion chemistry. This is the highest ener…
MIKROE Touchkey Click has four capacitive pads powered by TTP224, a touchpad detector IC.
Thermostat 4 Click is complete solution that senses the temperature of a physical system.
In 2015 we developed the BadgerStick as a fun and interactive way for people to learn about soldering and engage with SparkFu…
The Digilent BNC Adapter Board is a simple add-on board intended to be used with the Digilent Analog Discovery 2, which allow…
The main component of the Hz to V Click is the TC9400, a voltage-to-frequency and frequency-to-voltage converter from Microch…
Pressure 14 Click is a compact add-on board that contains a board-mount pressure sensor.
mikroBUS Shuttle is a small add-on board, which is intended to be used with Shuttle Click, in order to expand the mikroBUS™…
Got too much data for 10 measly segments? This kit contains a PCB and all the parts needed to build a 30-LED bargraph that ca…
Light pipe is very cool stuff. It transmits light along its length, like fiber optic cable, but it also "leaks" light along t…
The TLC5940 is a 16 channel PWM unit with 12 bit duty cycle control (0 - 4095), 6 bit current limit control (0 - 63), and a d…
LLC I2C Click can be utilized as the level converter for logic signals, which makes it a very useful Click board™.
SE051 Plug&Trust Click is a compact add-on board representing a ready-to-use IoT security solution.
Tilt 2 Click is a tilt sensor switch, which breaks the circuit when tilted to an angle of 45° or when shaken.
Solarbotic's Herbie the Mousebot is a 9-volt battery-powered, light-following robot that loves to chase flashlight beams. The…
**Replacement:** None. We do not have a direct replacement for this cable. This page is for reference only. This is a zinc d…
**Replacement:** None. We have stopped carrying the SCP1000, so we no longer carry the gasket. This page is for reference onl…
**Replacement:**[PRT-10453](http://www.sparkfun.com/products/10453). We are now selling ten-packs of screws. This page is for…
These 8" long stainless steel shafts have a diameter of 1/2". These shafts are solid, which makes them an ideal choice for ax…
These smooth (round) belts have a Durometer hardness of A70 and can withstand temperatures from -35 to 250 degrees F. Their e…
These side mount brackets can function as mounts for encaps for [Actobotics](https://www.sparkfun.com/pages/Actobotics) chann…
This is a simple LED-illuminated tactile button with an orange cap. It's just like a basic tactile button, but it lights up o…
The OpenMV M7 Camera is a small, low-power microcontroller board that allows you to easily implement applications using machi…
This is a 33mm round momentary push button similar to the ones you find on arcade games. Simple screw in design. Perfect for …
Introducing Newhaven Display's 7.0" HDMI TFT module complete with a capacitive touch panel. This display is part of the new H…
**Replacement:** None. There is no direct replacement for this item. This page is for reference only. This is the wall plate…
**Replacement:**[BOB-09945](http://www.sparkfun.com/products/9945). We've fixed the silkscreen labeling and consolidated the …
There are plenty of SparkFun Simons wandering around out there in the wild. A lot of the owners of those Simons are aware tha…
The RedBoard - BreadBoard Kit allows you to assemble your very own Uno-compatible development board on a breadboard. If you'v…
This one is for all you audio geeks out there. If you are going to play with MIDI accessories you'll likely need a cable. We …
This is a 1kg (2.2lb) reel of 3mm red PLA plastic filament for 3D printing. PLA is a great general purpose filament with grea…
The EasyDriver is a simple to use stepper motor driver, compatible with anything that can output a digital 0 to 5V pulse (or …
The Shapeoko XXL is a 3-axis CNC Machine kit that allows you to create your 2D and 3D designs out of non-ferrous metals, hard…