Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
The mbed boards are a series of ARM microcontroller development boards designed for rapid prototyping and this is breakout ma…
These 3" long stainless steel shafts have a diameter of 3/8". These shafts are solid, which makes them an ideal choice for ax…
This cable is 150mm long and has two 2.5mm spaced connectors at its ends.
**Note:** This was one of our April Fool's products for 2011. Sadly, it's not real. A soldering iron is an essential tool fo…
RS485 Isolator 2 Click features ADM2867E a 5.7 kV rms signal and power isolated full duplex RS-485 transceiver.
Too long have you suffered at the hem of shapeless, boxy t-shirts! Finally, we're stocking our popular SparkFun Tees in women…
The HMC6343 is a solid-state compass module with tilt compensation from Honeywell. The HMC6343 has three axis of magneto, thr…
Arduino Mega Click Shield is an extension for Arduino Mega and any other boards that share its pinout.
**Replacement:** None. We are no longer carrying this programmer, but check out our [programmers](http://www.sparkfun.com/cat…
This is 30AWG stranded black wire with a flexible silicone jacket. This wire is perfect for soldering and connecting any proj…
**Replacement: **None. We don't have a drop in replacement for this tool but there are still some options for you in the [Roo…
**Replacement:**[DEV-10915](http://www.sparkfun.com/products/10915). The new version of this board uses a sturdier right angl…
HDC1000 Click is a humidity (and temperature) measurement Click board™ carrying the HDC1000 sensor from TI.
**Replacement: **None. This product is in the middle of getting revised but we don't have a replacement yet. This page is for…
This is a small IR receiver module with built in lens, preamp, internal filter and demodulator. All in less than 8x3mm. Perfe…
The TAZ 4 3D printer from LulzBot represents the latest evolution in high performance desktop 3D printing technology. This 3D…
This is the low profile Raspberry Pi microSD card adapter from Adafruit. We know what you're thinking, "Why can't you just us…
The Helium Element Ethernet Access Point is the bridge between Atom modules and your preferred cloud platform. Atom devices c…
**Replacement:** None. We are no longer carrying these standoffs in our catalog. This page is for reference only. MicroRAX i…
These threaded aluminum clamping hubs are perfect for standard applications that need shafting or tubing 1" in diameter secur…
This pamphlet is a sales sheet for retailers to use for their retail displays. Have them for customers as informational take-…
**Replacement:** None. It's time for this product to step aside and make room in the catalog for even more cool stuff. This p…
This is a high-quality color CMOS camera module. Power the CM-32 module, hook up any display, monitor, or LCD screen with an …
The PocketLab Voyager is an all-in-one science lab that is capable enough for a professional engineer and simple enough for a…
These are blue 2" x 2" electroluminescent (EL) panels from ELastoLite®. These EL panels are highly flexible, waterproof, and…
**Replacement:** No direct replacement. VLSI has discontinued this chip and we will no longer be stocking it. Check out other…
**Replacement:**[DEV-11016](http://www.sparkfun.com/products/11016). The new version of this kit replaces the, now end-of-lif…
If you used BlinkM and you thought it was good, but needed something to temporarily blind your enemy, the MaxM is what you ne…
4x4 RGB Click is a matrix of 16 "intelligent" RGB elements, forming a 4x4 display screen.
This is a four wire cable with a 5 pin, 1.25mm pitch connector on one end. These cables are helpful if you're trying to simpl…
ECG 3 Click is a complete solution for ECG and HR application development, utilizing a specialized IC with a clinical-grade a…
This yellow EL Wire contains a special bendable wire core that allows you to articulate and mold your EL wire any way that yo…
SolidSwitch 2 Click is a compact add-on board that contains a load switching device.
A basic 12 button keypad for user input. The buttons are setup in a matrix format. This allows a microcontroller to 'scan' th…
DIGI POT 4 Click is a digitally controlled dual potentiometer, with the resistance of 10KΩ.
The SparkFun Lightning Detector adds lightning detection to your next weather station to make sure you are aware of any bad w…
MIC 2 Click is equipped with a small electret microphone, accompanied by a suitable pre-amplifying circuit.
**Replacement:**[COM-10963](http://www.sparkfun.com/products/10963). We are now carrying the EasyVR Shield, which is the same…
The LLC-SPI Click is a very useful Click board™ which can be utilized as the level converter for logic signals.
The SparkFun 9DoF IMU Breakout incorporates all the amazing features of the ICM-20948 into a Qwiic-enabled breakout board.
This is the fantastically easy to use sensor from [Maxbotix](http://www.maxbotix.com/). We are extremely pleased with the siz…
EL inverters allow you to drive EL wires. This particular EL inverter accepts 3V input and outputs 110VAC to drive EL wire. T…
You've always wanted to output analog voltages from a microcontroller, the MCP4725 is the DAC that will let you do it! The MC…
This is the new, weather resistant, field-hardened WR1 from [Maxbotix](http://www.maxbotix.com/). The XL series of this senso…
The SparkFun EL Sequencer is a board that contains an Arduino-compatible microcontroller, and circuitry for controlling up to…
**Replacement:** None. We don't have any of these boards left. This page is for reference only. This batch of the old UDB3 b…
Ninjaflex, or TPE (thermoplastic elastomer), is an exciting combination of sheer strength, low-temperature performance, abras…
This simple on-off switch is rated for 20A at 12V but who cares about all that, it looks way awesome. These toggle switches c…