Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
**Replacement:** None. This part is now end-of-life and we don't carry a direct replacement. Check out the rest of our [accel…
**Replacement:**[KIT-10003](http://www.sparkfun.com/commerce/product_info.php?products_id=10003). We switched to a better tri…
This is a breakout board for the SC16IS750, a handy chip used to convert I2C or SPI serial signals to a single-channel, high-…
**Replacement:**[DEV-09663](http://www.sparkfun.com/commerce/product_info.php?products_id=9663). This module has been updated…
MIKROE mikroProg for STM32 is a fast USB 2.0 programmer and hardware debugger based on ST-LINK v2.
These threaded aluminum standoffs are 1-1/2” long and have a thread pitch of 6-32, and an outer diameter of 0.25”. **N…
As you may already know, the Arduino Ethernet Shield allows an Arduino board to connect to the internet, which is awesome. It…
The Maximum Cubelet accepts many different inputs but only passes along the one with the greatest value. With a maximum block…
**The new version of this board can be found [here!](https://www.sparkfun.com/products/11812)** This is a simple to use, USB …
Conductive thread is a creative way to connect various electronics onto clothing. This thread can carry current for power and…
**Replacement:** None. We are no longer carrying this product in our catalog. This page is for reference only. Development b…
Ready to add some good vibes to your project? Look no further than the SparkFun Haptic Motor Driver. This board breaks out Te…
These hub-mountable aluminum sprockets can be used to drive wheels or other sprockets with 0.25” chain. They have 40 teeth …
**Replacement:** None. We are no longer building this board. This page is for reference only. The Spartan-3E Evaluation card…
MIKROE Fan 8 Click is a compact add-on board that represents a compliant fan controller.
This is a breakout board for the Bosch BMP180 high-precision, low-power digital barometer. The BMP180 offers a pressure measu…
This is the same product as the [Serial Enabled LCD Kit](http://www.sparkfun.com/products/10097). The difference is this vers…
Is your I2C bus not ACK'ing the way you expect? Do you need to discover a UART's mysterious baud rate? Or do you want to reve…
**Replacement:** None. We don't carry a direct replacement for this part but check out the rest of our [color LCDs](https://w…
This board is actually a pair of boards! We wanted to design a product that gave you the bare minimum amount of support circu…
Function generators are useful in a ton of applications from RF to embedded logic. They're not usually super cheap though. Go…
**Replacement:**[COM-08996](http://www.sparkfun.com/products/8996). These are gone but we still have the non-defective pads f…
The 4Duino is an Arduino compatible display module with built in 240x320 resolution TFT LCD Display with Resistive Touch, and…
**Replacement:**[TOL-10874](http://www.sparkfun.com/products/10874). We're switching things up, we've done away with some of …
The LilyPad SimpleSnap Protoboard is a new, easy way to create e-textiles projects with LilyPad that are modular and can be d…
LED Matrix with dual-color LEDs. This small matrix has both bright-red and bright-green LEDs built into one common cathode ho…
IR Click is an add-on board in mikroBUS™ form factor.
Hall Current Click is a high precision current sensor.
DIGI POT 5 Click is a digitally controlled quad potentiometer, with the resistance of 10KΩ.
The Tessel 2 is a development board with on-board WiFi capabilities that allows you to build scripts in Node.js. This Tessel …
RMS to DC Click is a board that is used to convert the RMS of the input signal into a DC voltage, with a value directly reada…
MCP25625 Click is a mikroBUS™ add-on board carrying a Microchip CAN controller with an integrated transceiver.
Charger 11 Click is a LiFePO4 (lithium iron phosphate) battery charger.
MIKROE nvSRAM Click is a compact add-on board that contains the most reliable nonvolatile memory.
The Slider 2 Click is a very accurate potentiometer Click board™, featuring a high-quality mechanical slide-action potentio…
Stepper 7 Click is a bipolar step motor driver.
The MLX90640 contains a 32x24 array of thermopile sensors creating, in essence, a low resolution thermal imaging camera. As t…
The microUSB Programming Adapter (μUSB-PA5) is a USB to Serial-TTL UART bridge converter which is very small and easy to use…
Ever wish your project could just speak up and *tell *you what's going on? Why not give it a voice? The Emic-2 Text-to-Speech…
There’s a lot of Raspberry Pi information going around lately. Whether it’s Pi A, A+, B, B+, or Pi 2 B, any forum will ha…
**Replacement:** None. We do not have a direct replacement for these. This page is for reference only. The LED Light Bar is …
The yellow 8BitDo Lite Bluetooth Gamepad is an ultra-portable controller made for 2D games & more.
**Replacement:** None. We are no longer carrying this style of solder tip but have a look at our [soldering tools](http://www…
**Replacement:** None. We are no longer carrying this LED breakout in our catalog. This page is for reference only. This is …
CO Click carries the MQ-7 gas sensor with high sensitivity to carbon monoxide.
**Replacement:**[COM-09650](http://www.sparkfun.com/products/9650). We no longer carry the rectangular package, however in mo…
**Replacement:** None. We do not have a direct replacement for this board. However, you might want to look at all of our [cur…
Your project can demand attention with these super loud car horns. Yes, they're actual car horns and they're every bit as lou…