Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
This red EL Wire contains a special bendable wire core that allows you to articulate and mold your EL wire any way that you w…
This pink EL Wire contains a special bendable wire core that allows you to articulate and mold your EL wire any way that you …
This orange EL Wire contains a special bendable wire core that allows you to articulate and mold your EL wire any way that yo…
This white EL Wire contains a special bendable wire core that allows you to articulate and mold your EL wire any way that you…
This simple adapter wire terminates on one end with a JST-PH Male connector, and a JST-SM Female connector on the other.
Bare Conductive has created intricate patterns on this three-pack of Printed Sensors for you to use in touch and proximity se…
This simple adapter wire terminates on one end with a JST-PH Female connector, and a JST-SM Male connector on the other.
The Mi-Light Remote Control is a 2.4GHz RF LED accessory that can change the color and dim non-addressable LED strips attache…
This board has [gone red](https://www.sparkfun.com/products/15093)! We've got a few of the original SparkX versions left. Sam…
Do you find yourself wishing that you had just a few more GPIO pins? What if you only need that _one more pin_? You _could_ a…
The RockBLOCK 9603 Accessory Cable is terminated with a simple 10-pin molex-style connector at one end and a bare wire pigtai…
These are skinny addressable 1-meter-long 5V RGB LED strips that come packed with 60 SK6812s. SK6812 LEDs are very similar to…
These are side-lit addressable 1-meter-long 5V RGB LED strips that come packed with 60 SK6812s.
These are skinny addressable 1-meter-long 5V RGB LED strips that come packed with a whopping 144 SK6812s.
Need to autonomously monitor for that specific color value? Want to hone in on that magenta ball? Or follow that aquamarine l…
This is a replacement soldering tip for the Weller WE1010 soldering station. It is a single flat type of soldering tip, measu…
Are you a traveler? Do you remove every ounce of extra weight from your gear? The SparkFun 1 meter Traveler microB cable is d…
Is your laptop covered in stickers that hide the dents? Do you put your equipment through its paces? The SparkFun 1 meter Rug…
The YARD Stick One SDR from Great Scott Gadgets is a sub-1 GHz wireless test tool controlled by your computer.
The SuzyQable allows developers, hobbyists, and others to quickly access debugging and developer features on ChromeOS and oth…
**Note:** This product is no longer in SparkX, but please check out it's [Red cousin](https://www.sparkfun.com/products/15089…
These are your basic, run-of-the-mill wire strippers from Techni-Tool with a comfortable grip making them an affordable optio…
These are high grade wire strippers from Techni-Tool with a curved grip making them an affordable option if you need to remov…
Add some serious data storage to your latest project with this 512Kbit (64KB) EEPROM. Some flash based microcontrollers (like…
The LPS25HB is an absolute pressure sensor which means that it has an internal vacuum as a reference. (As opposed to *differe…
This LCD Touchscreen HAT fits on top of the Raspberry Pi, practically form fitting on top of it so as not to compromise the o…
This product went [red](https://www.sparkfun.com/products/18354)! You can continue to order it as a normal SparkFun product. …
The black version of this board has been retired but the board has gone red! We upgraded to the SAMD21 on the [SparkFun Pro R…
Qwiic RF is a packet radio system that's designed for sending short packets of sensor data from one Qwiic bus to another. Mes…
The RPLIDAR A2 is the next generation of 360 degree 2D LIDARs. Each RPLIDAR can take up to 8000 samples of laser ranging per …
The TFMini is a ToF, Qwiic-enabled LiDAR sensor capable of measuring the distance to an object as close as 30 centimeters and…
The Rotary Dial Kit is designed to be a simple interface device for your project. Input is achieved using a rotating encoder …
This PowerFilm Solar Panel is a lightweight, paper thin, and flexible 10.5mA@7.2V power solution that can be easily integrate…
This 10 pack of PowerFilm Solar Panels are lightweight, paper thin, and flexible 10.5mA@7.2V power solutions that can be easi…
This PowerFilm Solar Panel is a large, paper thin, and flexible 200mA@15.4V power solution that can be easily integrated with…
This 5 pack of PowerFilm Solar Panels are large, paper thin, and flexible 200mA@15.4V power solutions that can be easily inte…
This PowerFilm Solar Panel is a lightweight and PSA & Kynar coated 50mA@4.8V power solution that can be easily integrated wit…
This 5 pack of PowerFilm Solar Panels are lightweight and PSA & Kynar coated 50mA@4.8V power solution that can be easily inte…
The GoPiGo Beginner Starter Kit from Dexter Industries is a complete robotics kit controlled by the Raspberry Pi 3 B+.
The GoPiGo Beginner Classroom Kit from Dexter Industries is a box of five robotics kits providing everything you need to outf…
The WT2003S makes playing MP3 files from an SD card dead simple! All you need to do is load your files onto the SD card, plug…
This product went [red](https://www.sparkfun.com/products/16531)! You can keep ordering as normal from SparkFun. The SGP30…
The PaPiRus is a HAT for the RPi that is capable of driving an ePaper display with ease by making use of the existing open so…
The PaPiRus Zero is an ePaper / eInk screen HAT designed for the Raspberry Pi Zero and the Raspberry Pi Zero W.
The TinyFPGA Programmer is a very simple USB-JTAG bridge designed to program bitstreams onto TinyFPGA A1 and A2 boards.
The TinyFPGA A2 board is a bare-bones breakout board for the XO2-1200 FPGA. Though small, the AX2 is an incredibly powerful b…
The TinyFPGA BX is a small FPGA board with all of the components and circuitry required for the FPGA to function, provided fo…
Arduino and Arduino compatible dev boards are an awesome tool for developing an idea quickly but, being development boards, t…