Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The SparkFun RTK Surveyor is an enclosed and ready to use GNSS receiver for centimeter-level positioning. No programming requ…
The IoT RedBoard is an ESP32 WROOM-equipped development board that has everything you need in an Arduino Uno with extra perks…
The SparkFun Pro Micro RP2040 is a low-cost, high performance board with flexible digital interfaces featuring the Raspberry …
The SparkFun Thing Plus - ESP32-C6 adds a powerful wireless development option to SparkFun's popular Thing Plus footprint.
The SparkFun ESP32-C6 Pocket Dev Board is built around a RISC-V single-core processor with 4 MB flash memory in a 1"x1" Qwiic…
The SparkFun ESP32-S2 WROOM Thing Plus is a highly-integrated, Feather form-factor development board equipped with the 2.4 GH…
The SparkFun DataLogger IoT comes preprogrammed to automatically log movement, GPS, and various pressure, humidity, and dista…
The PINECIL Soldering Iron Kit provides a compact powerhouse and everything you need to ignite your DIY dream.
The RedBoard Plus is an Arduino-compatible development board that has everything you need in an Arduino Uno with extra perks …
The 915MHz SiK Telemetry Radio V3 is a lightweight and inexpensive open source radio platform that can allow for ranges of 30…
The SparkFun NEO-M9N GPS Breakout with on-board chip antenna is a high quality GPS board with equally impressive configuratio…
These 0.3m cables have minor modifications that allow them to be be plugged into their ports regardless of orientation on the…
Need a USB-C cable that allows you to transfer data _and_ switch power? This is it!
The SparkFun MicroMod GNSS carrier board has the accuracy of GNSS Real Time Kinematics (RTK) with the flexibility of the Micr…
The PureThermal 3 FLIR Lepton Smart I/O Module is a hackable thermal webcam module for the FLIR Lepton Longwave Infrared (LWI…
Get started learning FPGA with this Alchitry Au Kit!
The Alchitry Au is the gold standard for FPGA development boards and it's possibly one of the strongest boards of its type on…
The SparkFun MicroMod GNSS Function Board takes everything we love about the ZED-F9P module from u-blox and combines it with …
If you are not needing a lot of power to start your FPGA adventure, or are looking for a more economical option, the Alchitry…
The SparkFun LiPo Charger Plus is the suped-up power option in the SparkFun line of single-cell lithium polymer (LiPo) batter…
The is the official USB Type-C Power Supply for the Raspberry Pi Model 4 B.
The Alchitry Au+ is the gold standard for FPGA development boards and it's possibly one of the strongest boards of its type o…
The SparkFun ESP32-S3 Thing Plus adds a powerful and versatile IoT development platform to the Feather-footprint Thing Plus l…
The SparkFun Thing Plus Matter is the first easily accessible board that combines Matter and SparkFun’s Qwiic ecosystem for…
The MyoWare® 2.0 Wireless Shield is designed to take in readings from the MyoWare 2.0 Muscle Sensor and wirelessly transmit …
The RED-V RedBoard from SparkFun is a low-cost, Arduino-compatible development board featuring the Freedom E310 which brings …
The Raspberry Pi 4 Desktop Kit (8GB) includes everything you need to turn any monitor with an HDMI port into a desktop PC.
SparkFun has teamed up with CircuitDojo to bring you the nRF9160 Thing Plus, featuring the powerful Nordic nRF9160 in a Feath…
1 Meter USB Type C to Type C cable USB 2.0 data transfer capabilities.
The new Raspberry Pi 27W USB-C PD (Power Delivery) Power Supply will deliver a maximum of 5.1V, 5A enabling the RPi 5 to powe…
Based on a new generation ARM Cortex M7, the Qwiic Tsunami extends polyphony to 25 mono or 13 stereo simultaneous uncompresse…
This Adapter allows you to run devices and cables with the classic USB Type A connector off a device or adapter with a USB Ty…
The SparkFun Artemis Thing Plus takes our popular Feather footprint and adds in the powerful Artemis module for ultimate func…
With a 32-bit ARM® Cortex®-M4 RISC core, the SparkFun STM32 Thing Plus brings power and precision to your projects.
The SparkFun Thing Plus - RP2040 is a low-cost, high performance board with flexible digital interfaces featuring the Raspber…
The SparkFun GNSS-RTK Accessory Kit gives you just what you need to start using your RTK board for your project.
This is a flexible USB-A to USB-C cable.
The RedBoard Artemis Nano is a miniature extremely versatile implementation of the Artemis module.
The SARA-R5 LTE GNSS Breakout is a robust development tool for the u-blox's impressive SARA-R510M8S LTE-M / NB-IoT module. Pe…
The SparkFun Digi XBee® Explorer USB-C is the perfect option for extensive XBee development functionality with quick (Qwiic)…
The SparkFun USB Host Shield contains all of the digital logic and analog circuitry necessary to implement a USB peripheral/h…
The SparkFun Digi XBee® Dev Board breaks out all the functionality of your Digi XBee module, with the ability to connect to …
The SparkFun expLoRaBLE Thing Plus is a Feather form-factor development board with the NM180100 system in package (SiP), from…
With this USB-C breakout you will be able to incorporate a vertical USB-C connector into your projects without needing to sol…
These 2m cables have minor modifications that allow them to be be plugged into their ports regardless of orientation on the U…
The RedBoard Artemis takes the incredibly powerful Artemis module from SparkFun and wraps it up in an easy to use and familia…