Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
This simple board breaks out a female USB type A connector's VCC, GND, D- and D+ pins to a 0.1" pitch header. If you want to …
This 10K trimmable potentiometer has a small knob built right in and it's breadboard friendly to boot!
4-digit 7-segment displays are really neat little devices, it's a shame that they can be so cumbersome to control. Well we've…
These 0.3m cables have minor modifications that allow them to be be plugged into their ports regardless of orientation on the…
The SparkFun AS7331 Qwiic Spectral UV Sensor measures UV radiation on three channels, UVA, UVB, and UVC, with high sensitivit…
Need a USB-C cable that allows you to transfer data _and_ switch power? This is it!
The SparkFun RFID USB Reader is a simple to use, USB to serial base unit for the ID-3LA, ID-12LA, and ID-20LA readers. Simply…
We know these look like a lot of our other LEDs, but they're not! These are PTH Addressable RGB LEDs with a WS2812 (or "NeoPi…
If you’re ready to step your Arduino game up from older 8-bit/16MHz microcontrollers, the SparkFun SAMD21 Mini Breakout is …
The SparkFun MicroMod GNSS carrier board has the accuracy of GNSS Real Time Kinematics (RTK) with the flexibility of the Micr…
Alligator clips (or Crocodile clips, if you prefer) are likely to be the most useful thing on your workbench besides the work…
The SparkFun Wireless Joystick Kit provides an easy way to control your next XBee project.
Here is a simple, low-cost, high quality servo for all your mechatronic needs. This servo is very similar in size and specifi…
The 4 GB Raspberry Pi 4 features the ability to run two 4k resolution monitors, to run true Gigabit Ethernet operations, all …
The RTL-SDR BLOG V3 is a low-cost software defined radio USB dongle.
The SparkFun Qwiic OLED 1.3in. is a Qwiic-enabled monochrome OLED that displays crisp white-on-black images and text.
The TCT40 distance sensor is great for non-contact distance readings from 2cm to 400cm. This unit adds a pair of Qwiic connec…
The SparkFun Arduino UNO R4 WiFi Qwiic Kit has everything you need to start using the UNO R4 WiFi and Qwiic ecosystem togethe…
The PureThermal 3 FLIR Lepton Smart I/O Module is a hackable thermal webcam module for the FLIR Lepton Longwave Infrared (LWI…
An assortment of colored wires: you know it's a beautiful thing. Six different colors of solid core wire in a cardboard dispe…
The LIDAR-Lite v3 LED is a small, lightweight, low-power optical ranging sensor with incorporated ANT profile wireless networ…
Sure, your flashing, chip-tune playing T-shirt is really cool at the party... but at some point you need to turn it off. And …
The SparkFun Inventor's Kit Bridge Pack for micro:bit was designed to provide you with an easy way to transform your m:b into…
The SparkFun Qwiic Single Relay provides you with the easiest to use relay yet, handling up to 5.5A at 240VAC for long period…
Get started learning FPGA with this Alchitry Au Kit!
The SparkFun OpenLog with Headers can store, or "log", huge amounts of serial data and act as a black box of sorts.
The SparkFun Qwiic Micro OLED Breakout is a Qwiic enabled version of our popular MicroView and micro OLED display!
The Alchitry Au is the gold standard for FPGA development boards and it's possibly one of the strongest boards of its type on…
This is an industrial grade DC Buck-Boost converter that inputs 8V to 40V and outputs 12V up to 3A or 36W. With tons of heats…
The SparkFun XBee Explorer Regulated takes care of the 3.3V regulation, signal conditioning, and basic activity indicators (P…
This is about 360 yards of conductive thread spun from stainless steel fiber and wound on a spool. You can use it as a creati…
If you are not needing a lot of power to start your FPGA adventure, or are looking for a more economical option, the Alchitry…
The SparkFun 8-Pin SOIC to DIP Adapter is a small PCB that lets you adapt SOIC packages into a DIP footprint. These tiny boar…
This new version uses an SMD 5x2 header. This is a simple to use USB AVR programmer. It is low cost, easy to use, works great…
These are very slim, extremely light weight batteries based on Lithium Ion chemistry. Each cell outputs a nominal 3.7V at 200…
The SparkFun OpenPIR is a highly customizable Passive Infrared (PIR) sensor based around the NCS36000 PIR controller. Passive…
Have you ever seen a [Weevil](https://en.wikipedia.org/wiki/Weevil)? It's a pretty under-appreciated beetle, so we thought it…
The GP-735 is a slim, ultra-high performance, easy to use GPS smart antenna receiver. With -162dBm tracking sensitivity and o…
The is the official USB Type-C Power Supply for the Raspberry Pi Model 4 B.
This ANT500 is a telescopic antenna designed for operation from 75 MHz to 1 GHz with a total length that is configurable from…
A simple flex sensor 4.5" in length. As the sensor is flexed, the resistance across the sensor increases. Patented technology…
This straight bar load cell (sometimes called a strain gauge) can translate up to 100g of pressure (force) into an electrical…
The SparkFun 8 Channel Level Shifter Breakout features the TXS0108E 8-bit, bi-directional logic level translator from Texas I…
This SMA to U.FL Cable is commonly used to attach WiFi, Bluetooth, or nRFxxx based devices to a 2.4GHz antenna. What makes th…
The Alchitry Au+ is the gold standard for FPGA development boards and it's possibly one of the strongest boards of its type o…
The GP-1818MK is a low-cost, high performance GPS module that provides position, velocity, and accurate timing via the NMEA-0…
The SparkFun Qwiic ToF Imager is built around VL53L5CX from ST Electronics; a state of the art, Time-of-Flight (ToF), multizo…
The SparkFun 5V/1A LiPo Charger/Booster is a no-nonsense circuit for generating one amp from a Lithium Polymer battery at 5V.…